Can I use Cyclone Pro as a debugger for K60 tower?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use Cyclone Pro as a debugger for K60 tower?

2,288件の閲覧回数
BasePointer
Contributor II

Hi,

 

I would like to order K60 tower.  We have Cyclone Pro. Can I use it on tower for debugging with CW? Or Do I have to order BDM pod?

 

 

Thank you.

0 件の賞賛
返信
2 返答(返信)

2,132件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

The Tower boards have an integrated OSJTAG debugger on the processor boards. This means that no external debugger is required.

 

There is also a standard Cortex debug + ETM connector which can be used by external debuggers which conform to this standard. The Cyclone Pro from P+E doesn't support ARM processors as far as I know (only HC08 HCS08, HC(S)12 and Coldfire+/V1).

 

Regards

 

Mark

 

0 件の賞賛
返信

2,132件の閲覧回数
BasePointer
Contributor II

Yes you are right, we need Cyclone MAX instead of Pro.

0 件の賞賛
返信