CPU MKL05Z32VFM4 on KL05z and Codewarrior 10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU MKL05Z32VFM4 on KL05z and Codewarrior 10.3

ソリューションへジャンプ
1,520件の閲覧回数
nguyennhatminh
Contributor IV

Hi pro!

I'm using FRDM-KL05Z with CPU MKL05Z32VFM4. (32 Pins)

I'm exploring the function Processor Expert of Codewarrior 10.3. But I'm facing with the issue is Processors that Codewarrior support is MKL05Z32VLF4 and MKL05Z16VLF4 (48 pins).

Please advise me on this issue.

Thank you,

Minh,

ラベル(2)
0 件の賞賛
返信
1 解決策
1,399件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

I think you are correct, in that version of CodeWarrior there was no support for KL05 in 32-pin package. To use this specific package you need to install the latest version of CodeWarrior, which is CW v10.6, or even CW v10.5 already supported it. Here is an image I took from a project in CW v10.5, and you can see the CPU type options:

KL05_package.png

Hope this helps!


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,400件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

I think you are correct, in that version of CodeWarrior there was no support for KL05 in 32-pin package. To use this specific package you need to install the latest version of CodeWarrior, which is CW v10.6, or even CW v10.5 already supported it. Here is an image I took from a project in CW v10.5, and you can see the CPU type options:

KL05_package.png

Hope this helps!


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信