COM port grayed out when write-memory failed case

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

COM port grayed out when write-memory failed case

1,313件の閲覧回数
saisyam_vangara
Contributor I

Hi ,

Currently, i am flashing binaries through blhost commands
Everything working fine but in write memory failed case i am unable to detect COMX in device Manager.
could you explain how to recover device and how to view COMX port active state in Device Manager.

currently, following below steps:
././bin/windows/bl host.bin -u -- get-property 1
././bin/windows/bl host.bin -u -- flash-erase-all-unsecure
././bin/windows/bl host.bin -u -- read-memory 0xb700 256
././bin/windows/bl host.bin -u -- flash-erase-region 0x0 0xb800
././bin/windows/bl host.bin -D -u -- write-memory 0x0 C:\tmp.bin
././bin/windows/bl host.bin -u -- reset

kindly provide a solution for this 

Thanks & Regards

SAISYAM VANGARA 

0 件の賞賛
返信
1 返信

1,262件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi SAISYAM VANGARA ,

  Please tell me what the kinetis chip you are using, give me your chip part number, please also tell me what the board you are using, the official board or the customer own designed board.

  Please share some screenshot about your problem, then I will help you to check the details.

Waiting for your updated information.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信