CMSIS-DAP Driver Installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS-DAP Driver Installation

11,868件の閲覧回数
pcpro178
Contributor III

I'm using Kinetis to try to load my project for a MKL17Z256VLH4 to a FRDM-KL26Z development board because our proto boards are not yet available.  I'm unable to get the debug session to launch.  From what I can tell I think that the CMSIS-DAP driver did not install, and I've been unable to find the download for the driver.  Any help here would be great.  This is the error I'm getting:

Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

0 件の賞賛
返信
3 返答(返信)

8,638件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Please download the driver from here https://os.mbed.com/handbook/Windows-serial-configuration

Regards,

Jing

0 件の賞賛
返信

8,640件の閲覧回数
pcpro178
Contributor III

Thanks, but when I try to install the driver I get this error: "The driver could not be installed. No mbed Microcontrollers were found."

0 件の賞賛
返信

8,640件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi Jim,

Was the board plugged in when you tried the driver installation?

Regards,

Chris

0 件の賞賛
返信