CMSIS DAP-DEBUG SWD problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS DAP-DEBUG SWD problem

2,263件の閲覧回数
niket_zope
Contributor III

Hello, I'm working on a project. 

Board - FRDM-KE15Z 

IDE - IAR 7.8

My question is when I put my code to debug (using on chip CMSIS Debugger) at the time of reinitialization of  the default pins When I reach  to SWD_IO and SWD_CLK pins the debug pointer gets misplaced. 

And I tried commenting the pins with there index inside my function and code works fine even in debug and release mode.

NOTE: the same code runs perfect when I debug via jlink debugger. I'm confused what could be the possible problem ?

and how to overcome it.

0 件の賞賛
返信
2 返答(返信)

2,163件の閲覧回数
niket_zope
Contributor III

Hi diego.charles,

Yes, You are correct that's my post only.  

0 件の賞賛
返信

2,163件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Niket_Zope,

I have noticed that you have a similar post 

Debug pointer lost while SWD_IO Pin initialization  (Please, correct me if that is not the case)

and that my colleague Kerry Zhou‌ is already helping you.  

I'll follow the progress on that post. 

Best regards, Diego. 

0 件の賞賛
返信