CLOCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLOCK

3,916 次查看
akshita_manwati
Contributor III

Hello

Are there any changes to be done to the clock when BLE Otac code is combined with CAN?

Thanks

Akshita Manwati

0 项奖励
回复
7 回复数

3,791 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

 There is the need to make some code modifications in order to add the CAn functionality in one of the Bluetooth LE projects. 

Are you following the AN12273? How are you adapting the code?

Regards,

Estephania 

0 项奖励
回复

3,791 次查看
akshita_manwati
Contributor III

Hello Estephania

I followed the above application node and merged my code. My CAN is working properly but the board is not advertising.

Thanks

Akshita

0 项奖励
回复

3,791 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Did you add the functionality that it starts automatically the advertisement ? Have you pressed the push buttons in order to advertise?

Regards,

Estephania

0 项奖励
回复

3,791 次查看
akshita_manwati
Contributor III

Hello

Yes I added the functionality of advertisement but the LED doesn't blink so even if I press the push button advertisement will not take place.

Thanks

Akshita 

0 项奖励
回复

3,791 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

You mention you are adapting the code of the application note, but that it's not adding the OTA support. When you ad the OTA support you need to add the alignment and use a special bootloader. Are you using it?

Regards,

Estephania

0 项奖励
回复

3,791 次查看
akshita_manwati
Contributor III

Hello

I have removed the functionality of the bootloader plus the issue has been resolved by changing the clock of the board.

Thanks and regards

Akshita

0 项奖励
回复

3,791 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

It is good that you were able to solve it.

Regards,
Estephania

0 项奖励
回复