I ported a project from KSDK 1.0 to 1.1 (in KDS 2.0) and am running into some trouble during the PDB initialisation.
Previously using KSDK 1.0, CLOCK_SYS_GetBusClockFreq() returned the correct 60MHz and I can calculate the correct PDB MOD value.
Now with KSDK 1.1 it returns 0.
I traced through the CLOCK_SYS_GetBusClockFreq() call but it goes through so many levels of lower level functions, I can't make sense of it anymore.
What's wrong?
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Marco,
You'd better don't port the KSDK1.0 project to KSDK1.1, they are not incompatible.
Sorry for the inconvenient for you !
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
In the mean time I found I needed the following in my hardware_init():
/* Setup board clock source. */
g_xtal0ClkFreq = 8000000U;
g_xtalRtcClkFreq = 32768U;
The bus clock now properly returns the 60MHz value I was expecting.
But I am stilling having trouble with the PDB when I enable the DMA trigger of the PDB.
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Marco,
The driver function between SDK1.0 and SDK1.1 are different , so it hared to porting .
So recommend create a new project about SDK 1.1 refer to the previous project.
BR
Alice