CLK OUT PIN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLK OUT PIN

Jump to solution
2,966 Views
nesrinemhiri
Contributor III

Hi all,

I use the FRDMK22FN512VLH12,i would like to measure the CLK out but i dont found in documentation one pin that via it i can affiche frequen cy in scope

can help me

Thank you

1 Solution
2,624 Views
santiago_gonzal
NXP Employee
NXP Employee

Yes, you also need to configure the pin muxing.

Se this great post from Derek Snell:

Verifying Internal Clocks in Kinetis

Regards,


Santiago

View solution in original post

0 Kudos
Reply
3 Replies
2,624 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello,

Search in the Reference Manual for CLKOUT. The pin is PTC2 and the register to configure that pin is the SIM_SOPT2.

Regards,

Santiago

2,624 Views
nesrinemhiri
Contributor III

i add this line:

#define SYSTEM_SIM_SOPT2_VALUE       0x00010020U        (clkout flash frequency)

,but i see anything in the scope!! should i configure the pin in other register ?

2,625 Views
santiago_gonzal
NXP Employee
NXP Employee

Yes, you also need to configure the pin muxing.

Se this great post from Derek Snell:

Verifying Internal Clocks in Kinetis

Regards,


Santiago

0 Kudos
Reply