CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

1,299件の閲覧回数
Flaviohpo
Contributor II

Hello all,

I'm using a 5V transceiver TJA1051T and the RX pin is 5V.

I tried to find the information if MKS20FN256VLL12 is compatible with 5V for CAN0_RX pin but I couldn't.

Does someone knows if I can connect directly? If not, a simple voltage divider should be enought? Any suggestions?

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,289件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I review the information from the Datasheet, and this did not mention the tolerance for the 5v. I recommend using a level shifter. 

Best regards,
Pavel