CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

1,303 Views
Flaviohpo
Contributor II

Hello all,

I'm using a 5V transceiver TJA1051T and the RX pin is 5V.

I tried to find the information if MKS20FN256VLL12 is compatible with 5V for CAN0_RX pin but I couldn't.

Does someone knows if I can connect directly? If not, a simple voltage divider should be enought? Any suggestions?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,293 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I review the information from the Datasheet, and this did not mention the tolerance for the 5v. I recommend using a level shifter. 

Best regards,
Pavel