CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?

1,289 次查看
Flaviohpo
Contributor II

Hello all,

I'm using a 5V transceiver TJA1051T and the RX pin is 5V.

I tried to find the information if MKS20FN256VLL12 is compatible with 5V for CAN0_RX pin but I couldn't.

Does someone knows if I can connect directly? If not, a simple voltage divider should be enought? Any suggestions?

Thanks

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,279 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I review the information from the Datasheet, and this did not mention the tolerance for the 5v. I recommend using a level shifter. 

Best regards,
Pavel