CAN/flexCAN communication on FRDM-K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN/flexCAN communication on FRDM-K64F

1,699件の閲覧回数
hms420
Contributor I
Setting up CAN communication on FRDM-K64F eval board? 
I am using SN65HVD230 CAN Board as a transceiver for CAN lines.
Using Loopback example code as a starting point.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,279件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Harshi,

Have you try to configure these pins as CAN function? These pins are disabled by default.

PTB18 PTB19.png

You can refer the flexcan interrupt_transfer example in SDK_2.1_MK64FN1M0xxx12.

SDK_2.1_MK64FN1M0xxx12 flexcan interrupt_transfer.png

The Flexcan Interrupt Transfer example is in twrk64f120m folder.(You need to download SDK_2.1_MK64FN1M0xxx12 or SDK_2.1_TWR-K64F120M. Don't select FRDM-K64F. )

Select TWR-K64F120M or MK64FN1M0xxx12.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信