CAN driver code example for Kinetis K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN driver code example for Kinetis K60

ソリューションへジャンプ
8,714件の閲覧回数
ekasuwartadi
Contributor II

Hello,

I would like to know if there is any code example for using CAN protocol for Kinetis K60 MCU. I have read the reference manual but it would be much easier to read some code examples.

Thank you.

ラベル(1)
タグ(2)
1 解決策
4,842件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Eka

Attached is CAN bus loop-back node sample code for your reference. Thanks.

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

4 返答(返信)
4,842件の閲覧回数
sruthyuk
Contributor I

Hello,

Anyone have a sample code for testing two CAN module communication (MK60FX512VLQ12 processor) in KDSK 2.0??

Best regards

sruthy

0 件の賞賛
返信
4,842件の閲覧回数
yarannan
Contributor III

Do you have CAN loop back sample code for KSDK1.1.0 ON KDS?

0 件の賞賛
返信
4,842件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Eka Suwartadi:

You did not mention which derivative of K60 family you are using.

If you have installed CodeWarrrior for MCU, then you can find some examples for CAN module in the next installation paths, but those are for 100 MHz K60:

- C:\Freescale\CW MCU v10.x\MCU\CodeWarrior_Examples\Kinetis_Examples\k60

- C:\Freescale\CW MCU v10.x\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512

Now, in the next link you can find a zip with a CAN example code provided by our colleague Augusto, in this case for the 120 MHz K60:

K60 120MHz CAN example

Hope this is somewhat useful!

/Jorge Gonzalez

4,843件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Eka

Attached is CAN bus loop-back node sample code for your reference. Thanks.

Hope my reply can help you.

Best Regards

Paul