CAN Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,687件の閲覧回数
josemartinez
Contributor III

Hi everyone,

I'm having a problem with the CAN component, I'm using Kinnetis K20, I'm adding this component to my project and I have configured, but when I do the compilation I have a problem en the file CAN.c which is inside the folder Generated_Code, I don't know why this problems appear, if someone knows why this can be possible, let me know please.

All errors are "identifier expected".

Thank you

I have attached an image with the configuration component.

Jose

ラベル(1)
0 件の賞賛
返信
1 解決策
4,560件の閲覧回数
josemartinez
Contributor III

Hi,

finally I managed to resolve the problem, I don't know why a GPIO component was creating this problem to the CAN component, these components are working in different ports. I have changed the GPIO component for a bitIO component and now it works perfectly both, the CAN and the bitIO component.

Thanks

Jose

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,560件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Jose,

What version of CW?

Regards

Luis

0 件の賞賛
返信
4,560件の閲覧回数
josemartinez
Contributor III

Hi Luis,

I'm using 10.4 version.

Thanks

Jose

0 件の賞賛
返信
4,561件の閲覧回数
josemartinez
Contributor III

Hi,

finally I managed to resolve the problem, I don't know why a GPIO component was creating this problem to the CAN component, these components are working in different ports. I have changed the GPIO component for a bitIO component and now it works perfectly both, the CAN and the bitIO component.

Thanks

Jose

0 件の賞賛
返信
4,560件の閲覧回数
Monica
Senior Contributor III

Jose,

Thanks a lot for sharing the workaround with us! Keep the good job up!

Best,

Monica.

0 件の賞賛
返信