CAN Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN Problem

跳至解决方案
4,741 次查看
josemartinez
Contributor III

Hi everyone,

I'm having a problem with the CAN component, I'm using Kinnetis K20, I'm adding this component to my project and I have configured, but when I do the compilation I have a problem en the file CAN.c which is inside the folder Generated_Code, I don't know why this problems appear, if someone knows why this can be possible, let me know please.

All errors are "identifier expected".

Thank you

I have attached an image with the configuration component.

Jose

标签 (1)
0 项奖励
回复
1 解答
4,614 次查看
josemartinez
Contributor III

Hi,

finally I managed to resolve the problem, I don't know why a GPIO component was creating this problem to the CAN component, these components are working in different ports. I have changed the GPIO component for a bitIO component and now it works perfectly both, the CAN and the bitIO component.

Thanks

Jose

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,614 次查看
LuisCasado
NXP Employee
NXP Employee

Hi Jose,

What version of CW?

Regards

Luis

0 项奖励
回复
4,614 次查看
josemartinez
Contributor III

Hi Luis,

I'm using 10.4 version.

Thanks

Jose

0 项奖励
回复
4,615 次查看
josemartinez
Contributor III

Hi,

finally I managed to resolve the problem, I don't know why a GPIO component was creating this problem to the CAN component, these components are working in different ports. I have changed the GPIO component for a bitIO component and now it works perfectly both, the CAN and the bitIO component.

Thanks

Jose

0 项奖励
回复
4,614 次查看
Monica
Senior Contributor III

Jose,

Thanks a lot for sharing the workaround with us! Keep the good job up!

Best,

Monica.

0 项奖励
回复