CAN ANY POST I2C1 CODE FOR MKL16Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN ANY POST I2C1 CODE FOR MKL16Z

1,416 Views
sreenathreddy
Contributor II

ack is not coming for me ,when i send slave address.

Original Attachment has been moved to: main.c.zip

Original Attachment has been moved to: i2c.c.zip

0 Kudos
Reply
1 Reply

1,339 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I would recommend customer to refer FRDM-KL26Z demo code, which provides accelmeter(MMA8451) via I2C module.

The demo project name is [FRDM_KL26ZDemo_freedom], which located at default path:

..\FRDM-KL26Z_SC\FRDM-KL26Z_SC_Rev_1.0\klxx-sc-baremetal\build\iar\FRDM_KL26ZDemo

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply