Building KBOOT Under KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building KBOOT Under KDS

2,595 Views
jeremyanderson
Contributor III

I'm trying to just get a compile, but when I import the projects I think I need I run into problems with my KDS configuration right away.  Here is the message (any ideas?):

Orphaned configuration. No base extension cfg exists for ilg.gnuarmeclipse.managedbuild.cross.config.elf.debug.1792027861

Tags (1)
0 Kudos
Reply
3 Replies

2,399 Views
mjbcswitzerland
Specialist V

Jeremy

Which source are you using?


It sound like either a KDS problem or you are opening an Eclipse project that is not compatible with KDS.

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 Kudos
Reply

2,399 Views
jeremyanderson
Contributor III

I imported the projects from NXP Kinetis Bootloader 2.0.0 targets\MK66F18\kds

0 Kudos
Reply

2,399 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jeremy Anderson

I'm using Kinetis Desing Studio 3.2 and the latest MCUBoot Software, I have not a problem to compile the code under Bootloader 2.0.0 targets\MK66F18\kds\frdm-k66f

Do you have the latest KDS version? also, could you try to check for updates under help tab?

Best regards

Jorge Alcala

0 Kudos
Reply