Building K70 MCU based data acquisition board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building K70 MCU based data acquisition board

Jump to solution
2,094 Views
phyprabab
Contributor I

Hello!

I am an EE student that is some what new to Freescale and MQX.  I am designing a board to do data acquisition and have chosen the K70 as the MCU to use (combination of ADC channels, DSP, and memory).  I am working with the K70 tower schematic removing various components and adding in necessary external ADC, power, etc. Intended functionality of the K70 I need to exploit includes SPI, parallel bus, internal ADCs, and internal PWM.  I am not currently interested in most of the components of the K70 tower board, so basically just stripping out unnecessary parts on the reference design.

I have been playing with the K70 tower board using MQX, awesome stuff.  I want my new board to run MQX (once its completed of course!).  Could anyone give me pointers, next steps, documentation or personal experiences in getting MQX running on their own board(s)?

Thank you for your time!

Labels (1)
0 Kudos
Reply
1 Solution
1,775 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Phy,

  Check out this thread, it'll help you out:  Re: MQX: Customizing a BSP for new hardware

  Easiest way is to keep the clock source the same (since that can take a bit to figure out). All the other stuff is pretty straight forward. There is an app note being worked on to flesh that out, but I don't have an ETA on that at the moment.

View solution in original post

0 Kudos
Reply
2 Replies
1,775 Views
Monica
Senior Contributor III

Hello Phy,

just checking if the reference helped out with your question. Don't forget to keep is posted! :smileyhappy:

Best regards,

Monica.

0 Kudos
Reply
1,776 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Phy,

  Check out this thread, it'll help you out:  Re: MQX: Customizing a BSP for new hardware

  Easiest way is to keep the clock source the same (since that can take a bit to figure out). All the other stuff is pretty straight forward. There is an app note being worked on to flesh that out, but I don't have an ETA on that at the moment.

0 Kudos
Reply