Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader

1,456 Views
Minu
Contributor I

I would like to know if same bootloader(MCUBOOT) is used for both the KL and KE series .Also I would like to know if customization is possible in bootloader.

0 Kudos
Reply
1 Reply

1,439 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello Minu,

Hope you are doing well.

The MCU bootloader serves as a common bootloader for all Kinetis devices. It provides a standard interface to the device via all of the available peripherals supported on a NXP Kinetis device.

For a customized interface, the MCU bootloader is provided as full source code that is highly configurable.

For more information about features, supported devices, guides and downloads, please visit the MCU Bootloader webpage.

Regards,
Eduardo.

0 Kudos
Reply