Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader

1,457件の閲覧回数
Minu
Contributor I

I would like to know if same bootloader(MCUBOOT) is used for both the KL and KE series .Also I would like to know if customization is possible in bootloader.

0 件の賞賛
返信
1 返信

1,440件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello Minu,

Hope you are doing well.

The MCU bootloader serves as a common bootloader for all Kinetis devices. It provides a standard interface to the device via all of the available peripherals supported on a NXP Kinetis device.

For a customized interface, the MCU bootloader is provided as full source code that is highly configurable.

For more information about features, supported devices, guides and downloads, please visit the MCU Bootloader webpage.

Regards,
Eduardo.

0 件の賞賛
返信