Bootloader FRDM k64f

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootloader FRDM k64f

4,086 次查看
c_querido
Contributor I

Hi guys,

I am having trouble doing the bootloader on my FRDM K64f board. I've done the steps on the site (https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?&tid=vanOpenSDA# FRDM-K64F)

by downloading the firmware which in my case is DAPLink and I also downloaded the Arm IDE toolchain.

I pressed the reset button for 1s while connecting to the pc and opens the folder FRDM-K64FD (: D), I never get BOOTLOADER Drive to copy the .bin file there. I have tried it on Win10 and Win 7 and the error holds.And the reset LED stills red color. 

In the images below you can check the messages I get when I try to bootloader:pastedImage_3.png

pastedImage_2.png

pastedImage_4.png

So I think this happens because the bootloader driver never comes to me.

But if the problem is different, please tell me how I can solve this problem please, it's for my masters these.

thanks

Catarina Querido

标记 (1)
0 项奖励
回复
4 回复数

3,943 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hi Catarina,

I'll be happy to assist you in finding out with your error message.

I'd like to know when you are downloading the binary file which one are you choosing for the FRDM-K64. I understand you want the DAPLink but which one are you choosing(so I can test it on my end).

pastedImage_1.png

Also which ARM IDE toolchain did you choose? pastedImage_3.png

If you can try again, please erase the files from the FRDM-K64 when you are in bootloader mode and drag the new binary you downloaded again. Let me know if during this process the files you described again appear during the copying of the binary.

Please let me know the results.

Best Regards,

Sabina

0 项奖励
回复

3,943 次查看
c_querido
Contributor I

Hi Sabina,

I apreciate a lot your help.

About the binary file I have tryed both DAPLink rev0244 and DAPLink rev0244

OpenSDA v2.2 Bootloader.

And about ARM IDE I choose ARM CMSIS-DAP serial drivers, and when I run it

they show this:

I choose this ARM IDE because I use MCUXpresso and whem I'm doing debbug I

choose MCUXpresso IDE LinkServer (inc. CMSIS-DAP) probes.

I think I never had been in bootloader mode because dont shows me a folder

said botloader to drop the files, I thonk Taht I'm always in the normal

mode in FRDM-K64F.

Thank you again,

Catarina Querido

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

Sem

vírus. www.avast.com

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

<#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>

nxf51209 <[email protected]> escreveu no dia sexta, 13/09/2019 à(s)

22:02:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Bootloader FRDM k64f

reply from Sabina Bruce

<https://community.nxp.com/people/nxf51209?et=watches.email.thread> in *Kinetis

Microcontrollers* - View the full discussion

<https://community.nxp.com/message/1206156?commentID=1206156&et=watches.email.thread#comment-1206156>

0 项奖励
回复

3,943 次查看
Sabina_Bruce
NXP Employee
NXP Employee

The image that you posted seems like you resolved the issue.

Were you able to resolve it?

Please let me know if so. 

Best Regards,

Sabina

0 项奖励
回复

2,611 次查看
milibaiocchi
Contributor I

Hi! I have the same problem. I'm using Windows 11. Could you help me?

0 项奖励
回复