Bootloader AN2295

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader AN2295

1,874 Views
andreytarakin
Contributor I

I ported the AN2295 bootloder to my chip (MK10DN512).

 

The bootloder linker configured

 

define symbol __ICFEDIT_region_ROM_start__      = 0x00000410;

define symbol __ICFEDIT_region_ROM_end__        = 0x00000AFF;

define symbol __ICFEDIT_region_RAM_start__      = 0x1fffff00;

define symbol __ICFEDIT_region_RAM_end__        = 0x1fffffff;

define symbol __ICFEDIT_region_RAM1_start__     = 0x20000000;

define symbol __ICFEDIT_region_RAM1_end__       = 0x200001ff;

define symbol IntVectTable_start__              = 0x00000000;

define symbol IntVectTable_end__                = 0x0000003f;

define symbol FlashConfig_start__               = 0x00000400;

define symbol FlashConfig_end__                 = 0x0000040f;

So in main project I do

 

define symbol __ICFEDIT_region_ROM_start__      = 0x00000B00;

define symbol __ICFEDIT_region_ROM_end__        = 0x00080000; //512K

And build to get s19 file.

 

I open Universal Bootlosder utility and press Connect.

I get the following message

 

Bootloader protocol version: 0x08 (Kinetis, read command supported)

CRC protocol NOT supported)

Bootloader version string: K10

System device ID: 0x10A [Kinetis K10] rev. 13

Kinetis Package: 144-pin

Number of memory blocks: 1

Memory block #1: 0x00004000-0x0007FFFF

Erase block size: 2048 bytes

Write block size: 128 bytes

Original vector table: 0x00000000-0x000003FF

New vector table: 0x00004000-0x000043FF

S19 Image Control.

Parsed S-record lines: 3577  Bytes total: 57192

Source address range: 0x0000-0xDF67

The S19 image also contains redirected vectors. The automatic redirection is skipped now.

WARNING! S19 image will not fit into available memory (at address 0x00000000)!

How should I configure the main project?

0 Kudos
Reply
1 Reply

1,656 Views
mjbcswitzerland
Specialist V

Hi Andrey

An application needs to be located where the boot loader expects to find it - therefore you need to see where that is in the boot loader configuration.

0xb00 would not be a valid address since it is in the first sector of the Flash (where the boot loader is) and so would not be possible.

Your application will also have a reset vector which will need to be located correctly - looking at the warning that you have I expect that you still have this at 0x0000000 which would be invalid since the boot loader is there (hence the overlap).


Regards

Mark

Serial Loader: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf

Better, faster, cheaper Kinetis developments for professional at: http://www.uTasker.com

0 Kudos
Reply