Boot pin for TWR-KL43Z48M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot pin for TWR-KL43Z48M

1,475 Views
tonymakkiel
Contributor III


Hi,

Where is boot pin for TWR-KL43Z48M on the board?  According to blhose User Guide this should be in document, KBTLDRDEMOUG. But cant find anything related to this particular board.

The other reference I could find on boot pin is in AN4997.pdf, which says

"When the BOOTCFG0 is low, the boot starts from the ROM location". Where is this BOOTCFG0?

Many Thanks,

Tony

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

1,345 Views
miduo
NXP Employee
NXP Employee

Hi,

BOOTCFG0 is the boot config function which is muxed with NMI pin.

0 Kudos
Reply

1,345 Views
tonymakkiel
Contributor III

Hi,

         I think I managed to get the board in boot mode inserting the usb, while reset pressed. But not sure whether it working. I copied the "hello_world.bin" in demo_apps to the mounted partition an reset the board. But no ACM interface is enumerated. Is there a way to make sure the board is still working?

0 Kudos
Reply