Baud Rate change on uc by MODBUS POLL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Baud Rate change on uc by MODBUS POLL

2,285件の閲覧回数
andréluis
Contributor II

Hi, my name is André. I'm using the software MODBUS POLL to read some data in an application. I make a circuit using the MKL26 to send/receive the data to USB to RS485. The problem is when i need to change the baudrate in the uc. I dont find the data when i change the baudrate in uc to work with other device. I send an image to show how i change the baudrate.

Thanks for the help.Sem título.png

0 件の賞賛
返信
2 返答(返信)

2,036件の閲覧回数
andréluis
Contributor II

Hi Fang Li. Its a customer board. I configure the UART with 19200, 8 bits, None parity and 1 bit to stop. The problem is when i change the baud rate in software, i need to verify this change e modify my baud rate in MCU. The problem is i dont find where in the software i see the change of data. I'm using the example usb cdc of the site MCU on eclipse. 

0 件の賞賛
返信

2,036件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

I am not sure if you are using the NXP evaluation boar or just customer board? And how did you config the UART port? You mean that it does not work at 38400 baud, however, please let me know if it work normal under 19200?

0 件の賞賛
返信