Looking for bootloader KV46 familly on MCUXpresso and not KDS3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for bootloader KV46 familly on MCUXpresso and not KDS3.0

Jump to solution
906 Views
merigotbertrand
Contributor III

I have developped many application and bootloader on KDS3.2

I use now MCUXpresso. Is there bootloader example I could use for kinetis FV4x ?

Thanks to all

bertrand 

1 Solution
761 Views
merigotbertrand
Contributor III

Hi Victor.

It helps

Thanks

View solution in original post

0 Kudos
2 Replies
762 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Bertrand,

The newest version of the SDK includes bootloader examples. You can download the SDK in the following link, under the section "Add software component" select mcu-boot so the SDK includes the bootloader examples. The default IDE selection is MCUXpresso. 

pastedImage_1.png

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

762 Views
merigotbertrand
Contributor III

Hi Victor.

It helps

Thanks

0 Kudos