Baremetal sample for Tower board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Baremetal sample for Tower board

ソリューションへジャンプ
2,938件の閲覧回数
renjithvamanan
Contributor III

Hi,

I am really sorry if this is a RYFM kind of question :smileyhappy:

My requirement is to start writing a bootloader fot MK60FN1M0 processor.

I have a tower board. To start with I need a sample app which is not running on MQX RTOS, to make the boot loader light.

Is there any bare metal hello world sample available that running on tower board.

I am looking for a sample to understand the processor initialization part etc that I may also have to incoporate in my boot loader.

Thanks,

Renjith

ラベル(1)
0 件の賞賛
返信
1 解決策
2,586件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Renjith:

You can find example codes in the package called "KINETIS_120MHZ_SC". This is available from the next link, under Snippets, Boot Code, Headers, Monitors, etc.

K60_120: Kinetis K60 Ethernet Crypto 120/150 MHz MCUs

And whenever you are in doubt and do not find answers in the community, please feel free to post you own question.

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,586件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Complete code solutions and prebuilt boot loaders are available here:

Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading

Regards

Mark

2,587件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Renjith:

You can find example codes in the package called "KINETIS_120MHZ_SC". This is available from the next link, under Snippets, Boot Code, Headers, Monitors, etc.

K60_120: Kinetis K60 Ethernet Crypto 120/150 MHz MCUs

And whenever you are in doubt and do not find answers in the community, please feel free to post you own question.

Regards!

Jorge Gonzalez

0 件の賞賛
返信
2,586件の閲覧回数
renjithvamanan
Contributor III

If somebody gets error saying "Undefined macro or opcode: export fpu_asm.s" while building the bare metal aplications,

Please refer to this problems building bare metal examples for kinetis K70

Regards,

Renjith

0 件の賞賛
返信