Baremetal sample for Tower board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Baremetal sample for Tower board

跳至解决方案
2,944 次查看
renjithvamanan
Contributor III

Hi,

I am really sorry if this is a RYFM kind of question :smileyhappy:

My requirement is to start writing a bootloader fot MK60FN1M0 processor.

I have a tower board. To start with I need a sample app which is not running on MQX RTOS, to make the boot loader light.

Is there any bare metal hello world sample available that running on tower board.

I am looking for a sample to understand the processor initialization part etc that I may also have to incoporate in my boot loader.

Thanks,

Renjith

标签 (1)
0 项奖励
回复
1 解答
2,592 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Renjith:

You can find example codes in the package called "KINETIS_120MHZ_SC". This is available from the next link, under Snippets, Boot Code, Headers, Monitors, etc.

K60_120: Kinetis K60 Ethernet Crypto 120/150 MHz MCUs

And whenever you are in doubt and do not find answers in the community, please feel free to post you own question.

Regards!

Jorge Gonzalez

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,592 次查看
mjbcswitzerland
Specialist V

Hi

Complete code solutions and prebuilt boot loaders are available here:

Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading

Regards

Mark

2,593 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Renjith:

You can find example codes in the package called "KINETIS_120MHZ_SC". This is available from the next link, under Snippets, Boot Code, Headers, Monitors, etc.

K60_120: Kinetis K60 Ethernet Crypto 120/150 MHz MCUs

And whenever you are in doubt and do not find answers in the community, please feel free to post you own question.

Regards!

Jorge Gonzalez

0 项奖励
回复
2,592 次查看
renjithvamanan
Contributor III

If somebody gets error saying "Undefined macro or opcode: export fpu_asm.s" while building the bare metal aplications,

Please refer to this problems building bare metal examples for kinetis K70

Regards,

Renjith

0 项奖励
回复