BOARD_BootClockVLPR in Clock Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOARD_BootClockVLPR in Clock Tool

1,485件の閲覧回数
shrejjjhh
Contributor III

Hi,

I am using MKL15Z128CAD4R. I am using Welcome | MCUXpresso SDK Builder  for clock configuration.

I have found clock configuration tool for BOARD_BootClockRUN. But there is no option for BOARD_BootClockVLPR.

How should I configure the clock for VLPR using this tool?

Regards,

Shrey

0 件の賞賛
返信
1 返信

1,371件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Shrey,

In the reference manual of the MKL15Z128CAD4R, section 5.5.2 you will find the following information. 

pastedImage_2.png

So, before entering VLPR mode you need to configure the frequency of the clocks according to the limitations of the VLPR mode. Since the frequency you need  in VLPR mode is slower than the one you are running normally, you need to divide the frequency of the clocks. You can do this with the help of MCUXpresso Config tools.

I recommend you to take a look into the User's Guide of MCUXpresso Config Tools, chapter 4 Clocks Tool.    

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信