BME support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BME support

跳至解决方案
3,490 次查看
dieterteuchert
Contributor IV

In my opinion, when it comes to ultra low power, it is about code size and cycle counting. The KL05-SC samples are somewhat disappointing in this respect. For example they do not use the port PCOR and PSOR functions properly and they do not show how to make use of the BME module. Did i miss something? Does the processor expert do it better, or one of the development environments? I am looking for samples or proposals on using the BME in a systematic fashion. At least there should be a set of macros like those mentioned in the reference manual.

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
2,747 次查看
dieterteuchert
Contributor IV

In the meantime i found the LQRUG_bme_ex1 sample, so i have to answer myself..

In that sample we have macro definitions for BME as inlinine C functions. Once i got those functions really inlined by the compiler, results were as expected: While the standard C implementations needed 13 or 14 systicks, BME achieved the same in 10 or 11 systicks. In general BME was faster by 4 systicks per operation, or 40 %.

With an optimizing compiler the things get confusing. For example once the processor has an address register for GPIOA_PDDR it may reuse it inside the benchmark for the logical operation on GPIOA_PDOR (which is nearby), while BME needs a completely new destination address.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,748 次查看
dieterteuchert
Contributor IV

In the meantime i found the LQRUG_bme_ex1 sample, so i have to answer myself..

In that sample we have macro definitions for BME as inlinine C functions. Once i got those functions really inlined by the compiler, results were as expected: While the standard C implementations needed 13 or 14 systicks, BME achieved the same in 10 or 11 systicks. In general BME was faster by 4 systicks per operation, or 40 %.

With an optimizing compiler the things get confusing. For example once the processor has an address register for GPIOA_PDDR it may reuse it inside the benchmark for the logical operation on GPIOA_PDOR (which is nearby), while BME needs a completely new destination address.

0 项奖励
回复
2,747 次查看
Monica
Senior Contributor III

Dieter,

Thanks for sharing your updates, that's very valuable!

Best regards,

Monica

0 项奖励
回复