BLE on Hexiwear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE on Hexiwear

1,453 Views
microbob
Contributor I

Hello, I have a few question concerning the BLE function on the Hexiwear.

  • Is there an API or library for using the KW40z BLE SoC on the Hexiwear?
  • Is the BLE SoC's transmission being sent to a serial port or somewhere else?
  • Can the BLE send its data over the UART to a serial port?
  • Can you use a  programming language like Java to determine the BLE RSSI from the Hexiwear? If not, can the Hexiwear determine its own RSSI with the paired device?

Thank you in advance for helping me!

Tags (2)
0 Kudos
Reply
0 Replies