BIG PROBLEM! K22FX512 continue to reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BIG PROBLEM! K22FX512 continue to reset

2,242 Views
ypkdani
Contributor III

Hello,

i have develop a new embedded board with the MK22FX512VLL12. I have put a pull-up of 10kohm on the reset pin but when i try to program this micro for the first time the reset pin continue to oscillate. 

pastedImage_1.png

i have try with the segger commander with the command erase and unlock kinetis but nothing. I can't erase the memory. I have read some post that speak about this problem but i didn't find a solution. I use a EDU Segger Jlink.

This happen on all board

Thanks

0 Kudos
Reply
3 Replies

2,018 Views
ypkdani
Contributor III

Ok, for two board i have solve using jlink commander:

  1. run command "r0" to set reset pin to 0
  2. give "unlock kinetis"
  3. give "erase MK22FXAXXX12"

monday i will try with other board

0 Kudos
Reply

2,018 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Daniel Cortellazzi

Actually this is not a problem, it is telling you that there is anything in the flash memory, so when your device try to fetch a instruction from the internal flash and it doesn't find anything it cause a hard fault and it reset, when the process repeat, it reset again, and it stock in this loop.

If you flash a program in this devices the reset line should behave normal.


Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,440 Views
Lily_cheng
Contributor I

I had the same promblem.

after saveral reset K22FX512 continue to reset.
sometimes JLINK can't connect to  K22FX512.

yes, you are right ,the data in flash has some error which cause this promblem, but the question is , why flash's data error after reset ?

I read data when sometimes connect success, the data goes to FF.

Could you explain why the data goes to FF after reset? 

0 Kudos
Reply