BAUD RATE CHANGE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BAUD RATE CHANGE

1,621 次查看
odilbekurmonov
Contributor I

I am using mkw01z128 boar. It has default baud rate on uart0,1,2 - 115200. But I need another baud rate. How to change it ?

0 项奖励
回复
1 回复

1,444 次查看
isaacavila
NXP Employee
NXP Employee

Hello Odilbek

In App.c file you can find the App_init function (line 208) in which serial interface is initialized:

    /* Initialize the serial terminal interface so that we can print out status messages */

    Serial_InitInterface(&interfaceId, APP_SERIAL_INTERFACE_TYPE, APP_SERIAL_INTERFACE_INSTANCE);

    Serial_SetBaudRate(interfaceId, gUARTBaudRate115200_c);

    Serial_SetRxCallBack(interfaceId, UartRxCallBack, NULL);

Serial_SetBaudRate function does configure baud rate, if you want to change baud rate, you should replace gUARTBaudRate115200_c parameter by anyone of followings:

typedef enum{

    gUARTBaudRate1200_c   =   1200UL,

    gUARTBaudRate2400_c   =   2400UL,

    gUARTBaudRate4800_c   =   4800UL,

    gUARTBaudRate9600_c   =   9600UL,

    gUARTBaudRate19200_c  =  19200UL,

    gUARTBaudRate38400_c  =  38400UL,

    gUARTBaudRate57600_c  =  57600UL,

    gUARTBaudRate115200_c = 115200UL,

    gUARTBaudRate230400_c = 230400UL

}serialUartBaudRate_t;

Save changes and re-compile the project.

I hope this can help you!

Best Regards

Isaac Avila

0 项奖励
回复