AsynchroSerial problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AsynchroSerial problem

Jump to solution
3,820 Views
andredehn
Contributor I

Hello together!

I have a problem with the AsynchroSerial component, to include the a UART-Value.

The Processor named MKL15Z128VFM4.

Everything works, except for these error messages:

1.)

ERROR: at line 267: List name undefined: UART1_Divider_Setting (file: Drivers\Kinetis\Serial_LDD.rgi)    tunnel        ASerialLdd1    Processor Expert Problem

2.)

ERROR: at line 267: Unknown macro  (file: Drivers\Kinetis\Serial_LDD.rgi)    tunnel        ASerialLdd1    Processor Expert Problem

3.)

ERROR: at line 268: Error in expression: For input string: "%[1,UART1_Divider_Setting]" (file: Drivers\Kinetis\Serial_LDD.rgi)    tunnel        ASerialLdd1    Processor Expert Problem


Someone has an idea what I might have done wrong or
what could I do differently?


The same Error appears if I use the Serial_LDD to include a UART


I tested with the KL15Z128VLK4 again with the same result.

I also try to include this at the MK60DN256VLQ10 and it WORKS!




many greetings


André

Labels (1)
0 Kudos
Reply
1 Solution
3,369 Views
vfilip
NXP Employee
NXP Employee

Hello,

I was not able to reproduce it. Could you please post here the ProcessorExpert.pe file from your project in order to reproduce it? What version of CW or DriverSuite do you use?

For now, please close the Configuration Registers view, it should help to avoid the problem.

Note:

Please post future ProcessorExpert related question on Processor Expert Software forum:

Processor Expert Software

best regards

Vojtech Filip

Processor Expert Support Team



View solution in original post

0 Kudos
Reply
4 Replies
3,369 Views
sneaky07
Contributor I

Hi I'm getting this error using CW 10.3 with the Freedom MKL25Z board.  I'm using the Serial_LDD component as well with Processor Expert.  Andre, could you share exactly what you did to get rid of the errors?  This is the only thread that I have seen this issue in.  If you know of another please post.

Thanks,

John

0 Kudos
Reply
3,370 Views
vfilip
NXP Employee
NXP Employee

Hello,

I was not able to reproduce it. Could you please post here the ProcessorExpert.pe file from your project in order to reproduce it? What version of CW or DriverSuite do you use?

For now, please close the Configuration Registers view, it should help to avoid the problem.

Note:

Please post future ProcessorExpert related question on Processor Expert Software forum:

Processor Expert Software

best regards

Vojtech Filip

Processor Expert Support Team



0 Kudos
Reply
3,369 Views
andredehn
Contributor I

Thanks for the answer, now it works.



But interesting is why he even brings the error only:
ProcessorExpert.pe - Pastebin.com


Thanks a lot.



0 Kudos
Reply
3,369 Views
vfilip
NXP Employee
NXP Employee

Hello,

I was not able to reproduce your issue above our current files, so I assume that the fix of this problem will be published in CW V10.3 production (end of Q4 2012).

We are sorry for inconvenience.

best regards

Vojtech Filip

Processor Expert Support Team


0 Kudos
Reply