Any free modbus library kinetis k64?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any free modbus library kinetis k64?

Jump to solution
2,408 Views
albertolubeiro
Contributor III

Hi everybody,

Anybody knows where can i get a free modbus library?

I am working with Kinetis K64 over KDS IDE.

I am also working with MQX.

Thanks and best regards

0 Kudos
Reply
1 Solution
1,738 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Alberto,

You may find useful following post.

How to: KSDK-based Modbus RTU Packet Assembler in MQX


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,739 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Alberto,

You may find useful following post.

How to: KSDK-based Modbus RTU Packet Assembler in MQX


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply