Android Play application: Xtrinsic Sensor fusion toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android Play application: Xtrinsic Sensor fusion toolbox

7,960件の閲覧回数
simonmarkham
Contributor I

If you have an Android device and go to Android Play, you can download Freescale's Xtrinsic Sensor fusion toolbox.

In the documentation the FRDM KL25Z and other KL series are mentioned using a FRDM-FXS-MULTI freedom sensor shield.

I can't find any data on this shield, has it been released yet? does anyone else know about it?

Yours Simon M.

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

7,314件の閲覧回数
peter_fenn
Contributor V

Simon

Also included in Freescale Xtrinsic Sensor Fusion App is built-in support for Avnet's "Wi-Go" sensor board for which applicable FRDM-KL25Z application software (for full tilt-compensated eCompass function as well as Wi-Fi communication with the Freescale App) is available to developers.


More detail on the Avnet Wi-Go board (and reference software) is available here:
http://em.avnet.com/wi-go

Regards

Peter Fenn

Xtrinsic Sensor Fusion App.jpg

0 件の賞賛
返信

7,314件の閲覧回数
simonmarkham
Contributor I

Hi Peter,

I saw that, but I was put off by the import shipping & taxes to the UK, but I might bite the bullet and get it anyway...

Yours Simon M.

0 件の賞賛
返信

7,314件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

Simon,

It hasn't been released yet.  Current status is that we did a limited, pre-production, build to do basic validation of the design.  Those are the boards shown at various trade shows last week.  I'm expecting general availability in August.

Regards,

Mike Stanley

7,314件の閲覧回数
simonmarkham
Contributor I

Hi Mike,

Can you give any info on it yet?

Yours Simon M.

0 件の賞賛
返信

7,314件の閲覧回数
michaelestanley
NXP Employee
NXP Employee

I refer to this as our "kitchen sink board". Tentatively, we plan to include options for:

  • Freescale gyro (still to be announced)
  • FXOS87000CQ Combo sensor (3-axis mag + 3-axis accel)
  • MMA9553 Pedometer
  • MAG3110 Magnetometer
  • MMA8562FC Accelerometer
  • MPL5115A2 Pressure Sensor
  • Visible light sensor (non-Freescale)
  • FXLS84710 SPI Accelerometer
  • BlueRadios Bluetooth module

The board will probably be manufactured with different combinations of the above.  Specific configurations and prices are still TBD.

7,314件の閲覧回数
simonmarkham
Contributor I

Roll on August!

I can see this being popular with Autonomous flight folk.

(a GPS would be the cherry on top! )

Yours Simon M.

Keep me informed please Michael

0 件の賞賛
返信

7,314件の閲覧回数
albertocarrillo
Contributor I

Hello

Freedom Sensor board is now released

FRDM-FXS-MULTI-B Product Summary Page

Regards

Alberto

0 件の賞賛
返信