Analogue reference voltage pin in MKL03Z8VFG4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Analogue reference voltage pin in MKL03Z8VFG4

ソリューションへジャンプ
1,919件の閲覧回数
mrinal
Contributor I

Hi!

My application requires sampling of three analogue lines and transmitting the results via serial line.

I am thinking to use MKL03Z8VFG4.

But I am not sure about the analogue reference voltage pin. The datasheet says (on page number 34):  "For packages without dedicated VREFH and VREFL pins, VREFH is internally tied to VDDA, and VREFL is internally tied to VSSA".

The 16-pin package does not have dedicated VREFH and VREFL. So the reference pin should be internally tied to VDDA. However the package does not even have a VDDA pin. As far as power is concerned, there are only two pins i.e. VDD and VSS.

What does this mean? Does it mean that VDDA and VDD are the same? The datasheet also mentions that there is a  1.2V on chip voltage reference. How to use this reference?

Please help...

Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,786件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mrinal Mani,

    1. Analog reference pin

pastedImage_1.png

pastedImage_2.png

So, VREFH, VDD, VDDA is the same pin in VDD pin. VREFL, VSSA, VSS is the same pin in VSS.

2.  1.2v on chip voltage refernce

VREF_OUT is in pin PTB2, it can output 1.2V.

 More details, please refer to the KL02 reference manual, Chapter 30 Voltage Reference (VREF)

Wish it helps you!

If you still have question, please let me know~!


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,786件の閲覧回数
mrinal
Contributor I

Hi!

Thanks for the reply. The reference manual solves the purpose. It mentions how to use the internal 1.2V source as VREF for the ADC.

Regards

Mrinal

0 件の賞賛
返信
1,787件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mrinal Mani,

    1. Analog reference pin

pastedImage_1.png

pastedImage_2.png

So, VREFH, VDD, VDDA is the same pin in VDD pin. VREFL, VSSA, VSS is the same pin in VSS.

2.  1.2v on chip voltage refernce

VREF_OUT is in pin PTB2, it can output 1.2V.

 More details, please refer to the KL02 reference manual, Chapter 30 Voltage Reference (VREF)

Wish it helps you!

If you still have question, please let me know~!


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信