After building MQX6.2 IAR IDE does not have the MQX tool bar tab as in the class.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

After building MQX6.2 IAR IDE does not have the MQX tool bar tab as in the class.

2,076 次查看
captmark
Contributor I

Hello,   

 

           In class with the K40 tower using my personnel lap top with a 30day eval from IAR I had no problem compiling and running all the labs. At work I can complie Lab 1 which does not use MQX rtos. If I try to run any lab using MQX I cannot compile the code.  Also I do not see the MQX tool bar tab that showed up with the 30 day eval.

              My IAR is ver 6.2 and when I batch build the MQX6.2 softwate I get no errors.

 

Can any one think of what could be wrong?

 

Thanks  Capt Mark

 

 

 

0 项奖励
回复
3 回复数

1,869 次查看
tr9
Contributor II

Hello Capt,

 

I am having a similar problem. Did you ever get an answer?

0 项奖励
回复

1,869 次查看
captmark
Contributor I

No I have not. I will be going to thr FTF in two weeks but hope to find answer before.

 

Capt

0 项奖励
回复

1,869 次查看
anthony_huereca
NXP Employee
NXP Employee

What kind of compile errors did you get? That can help narrow down what went wrong.

0 项奖励
回复