Adding two FRDM- KL25Z Microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding two FRDM- KL25Z Microcontroller

1,305件の閲覧回数
khalidal-dawoud
Contributor I

What is the best way to use two microcontrollers in autonomous car with out any conflict in the orders? The first microcontroller will be used for the speed process, and the other one will be used for the two line cameras? 

0 件の賞賛
返信
1 返信

1,218件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The KL25 UART module supports LIN bus, which could be used as a LIN slave in CAR network.

NXP provides the LIN2.x and SAE J2602 Stack(REV v4.5.9), which supports KEA product so far.

If customer consider the communication speed, customer could select a MCU with CAN module.

best regards,

Mike

0 件の賞賛
返信