Adding two FRDM- KL25Z Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding two FRDM- KL25Z Microcontroller

1,315 Views
khalidal-dawoud
Contributor I

What is the best way to use two microcontrollers in autonomous car with out any conflict in the orders? The first microcontroller will be used for the speed process, and the other one will be used for the two line cameras? 

0 Kudos
Reply
1 Reply

1,228 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The KL25 UART module supports LIN bus, which could be used as a LIN slave in CAR network.

NXP provides the LIN2.x and SAE J2602 Stack(REV v4.5.9), which supports KEA product so far.

If customer consider the communication speed, customer could select a MCU with CAN module.

best regards,

Mike

0 Kudos
Reply