About the SRAM locations in KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the SRAM locations in KL25Z

跳至解决方案
2,360 次查看
tagerud
Contributor I

When reading the user guide for M0+ (https://static.docs.arm.com/dui0662/a/DUI0662A_cortex_m0p_r0p0_dgug.pdf) on page 22 it says that SRAM starts at address 0x2000_0000. However, in the KL25 reference manual, the SRAM is divided in upper and lower sections, where the lower starts at 0x1FFF_F000 (for my 128 KB device). This would put it in the code section, according to the user guide. 

I would just like to understand why this is the case? According to an answer to this question: Why is SRAM split, and what does it mean?, the M0+ does not have separate busses for upper and lower SRAM, so I don't really have to think about it. But even so, why go against the CPU memory model?

Edit: Corrected lower adress.

1 解答
2,235 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear [email protected]‌,

All the Kinetis Devices has the SRAM memory partitioned this way, in the case of the K series  the reason is shown in the next application note (Optimizing performance on Kinetis K-series MCUs AN4745):

 

All Kinetis K-series devices include two blocks of on-chip SRAM. The first block (SRAM_L) is mapped to the CODE bus, and the second block (SRAM_U) is mapped to the system bus. The memory itself can be accessed in a single cycle, but because instruction accesses to the system bus incurs a one clock delay at the core, SRAM_U instruction accesses take at least two clocks.

 

And for example in the KL8x, In LLS2 and VLLS2 the 32KB region of SRAM_U based at 0x2000_0000 are powered.

 

So this is a convention in the Kinetis MCUs.

 

I hope this information helps you.

 

Best Regards,

Alexis Andalon

在原帖中查看解决方案

2 回复数
2,236 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear [email protected]‌,

All the Kinetis Devices has the SRAM memory partitioned this way, in the case of the K series  the reason is shown in the next application note (Optimizing performance on Kinetis K-series MCUs AN4745):

 

All Kinetis K-series devices include two blocks of on-chip SRAM. The first block (SRAM_L) is mapped to the CODE bus, and the second block (SRAM_U) is mapped to the system bus. The memory itself can be accessed in a single cycle, but because instruction accesses to the system bus incurs a one clock delay at the core, SRAM_U instruction accesses take at least two clocks.

 

And for example in the KL8x, In LLS2 and VLLS2 the 32KB region of SRAM_U based at 0x2000_0000 are powered.

 

So this is a convention in the Kinetis MCUs.

 

I hope this information helps you.

 

Best Regards,

Alexis Andalon

2,235 次查看
tagerud
Contributor I

That makes perfect sense. Thank you for the source!

0 项奖励
回复