About flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About flash memory

1,715 Views
Sourdev
Contributor II

I am using S9KEAZN64AMLC mcu (Custom Board).

Is there any status bit in FLASH to indicate that flash is in process (Erase and write)?  like the FLASH BUSY status bit ? 

How do we know that FLASH is completed erase or write?

0 Kudos
Reply
1 Reply

1,679 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please read the 18.3.9.9 Erase flash sector command of KEA64RM.

18.3.9.9 Erase flash sector command.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply