About VREF pin for MKM14Z128?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About VREF pin for MKM14Z128?

2,360件の閲覧回数
mercysun
Contributor I

For SD ADC use in MKM14Z MCU,It’s not easy find the Pin VREF input properties.

How about the VREF pin input range if use an external voltage reference for SD ADC?

If use internal reference (1.2V bandgap),what's SD ADC accuracy?

What's the condition for SD ADC reach 24bit?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,108件の閲覧回数
apanecatl
Senior Contributor II

You can find a detailed description of the VREF submodule and pin in the device's reference manual, check Chapter 3: Chip configuration and look for the VREF section, if you need to use an external reference you will have to use the VREFH pin to set the upper voltage reference.

0 件の賞賛
返信

2,108件の閲覧回数
mercysun
Contributor I

Thanks for your quickly response!

For the 24 bit sigma delta ADC,

In RM Chapter 3, Case III, its only tell VREF use 1.2V reference, i'd like to know for use an upper(>1.2V) voltage reference is ok?  if it's ok ,for a 3.3V external  voltage reference, what's the SD ADC input range? still 1Vpp or >3Vpp?

In datasheet,6.4.1 ,VREFH input range is 1.13~VDDA, Is VREFH  an output pin when use an external voltage reference?

Thanks

0 件の賞賛
返信

2,108件の閲覧回数
apanecatl
Senior Contributor II

VREF can only provide a 1.2V + trimm (.05mV per step) you CANNOT connect VREFout to an external power supply; if you need to use a higher voltage reference for any of the available ADCs you need to use the VREFH pin as the voltage reference, this pin can be connected to an external power supply which can range from 1.13 - VDDA, the ADC range remains the same with the exception that if you use an offset level you must take it into consideration. As I mentioned before, VREFH is an input pin which can be connected to an external power supply.

0 件の賞賛
返信