About USB Host and Device configurations on K21

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About USB Host and Device configurations on K21

1,625件の閲覧回数
rahulhirve
Contributor II

Hi all,

 

I am trying to use USB host and device configuration dynamically on k21 system. I am polling on a USB ID pin and configure host or device based on ID pin detection.

 

But I need this dynamically happen, so when system is running if I should able to change configuration from device to host or vise-versa.

 

Currently I can configure system either to host or to device once at time of boot sensing ID pin. But when I change ID pin while system is running then it does not reconfigure and fails for any data communication.

 

Any suggestions?

 

Attached in my init code APIs

 

Thanks,

Rahul 

Original Attachment has been moved to: usb_code.c.zip

0 件の賞賛
返信
1 返信

1,245件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rahul,

I'd like to highly recommend that you should choose USB On-The-Go mode which can determine the role of the device based on hardware signal,

and then initializes the device in the appropriate mode of operation (host or peripheral) based on how it is connected.

The KSDK 1.2 also contains the USB On-The-Go demo for K21 and please go ahead to download through the link as below.

Software Development Kit for Kinetis MCUs|Freescale
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信