About MKV46F256VLL16 ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MKV46F256VLL16 ports

1,576件の閲覧回数
takeuchi_kazuhi
Contributor II

About MKV46F256VLL16 ports

If Disable is assigned in the ALT default setting, please tell me the value after releasing RESET.
pull up? or pull down? or Hi-Z?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,477件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

With the exception of the JTAG pins, during reset the digital I/O pins got to a disabled(high impedance) state.

When the Pin Muxing mode is configured for analog or is disabled, all the digital functions on that pin are disabled. This includes the pullup and pulldown enables, output buffer enable, input buffer enable, and passive filter enable.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,477件の閲覧回数
takeuchi_kazuhi
Contributor II

Hi Da Li

Thank you for your prompt response.
I was able to understand.

Best regards

Takeuchi

0 件の賞賛
返信