About MKV46F256VLL16 ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MKV46F256VLL16 ports

519 Views
takeuchi_kazuhi
Contributor II

About MKV46F256VLL16 ports

If Disable is assigned in the ALT default setting, please tell me the value after releasing RESET.
pull up? or pull down? or Hi-Z?

Labels (1)
0 Kudos
Reply
2 Replies

420 Views
nxf56274
NXP Employee
NXP Employee

Hi,

With the exception of the JTAG pins, during reset the digital I/O pins got to a disabled(high impedance) state.

When the Pin Muxing mode is configured for analog or is disabled, all the digital functions on that pin are disabled. This includes the pullup and pulldown enables, output buffer enable, input buffer enable, and passive filter enable.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

420 Views
takeuchi_kazuhi
Contributor II

Hi Da Li

Thank you for your prompt response.
I was able to understand.

Best regards

Takeuchi

0 Kudos
Reply