About MKV46F256VLL16 ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MKV46F256VLL16 ports

1,921件の閲覧回数
takeuchi_kazuhi
Contributor II

About MKV46F256VLL16 ports
Is it possible to output both FLEX PWM and SPI to the terminal?
What settings should I make when possible?

4 返答(返信)

1,815件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Takeuchi,

 

I am sorry but I do not understand your question quite well. Could you please be more specific regarding what are you trying to accomplish? Which terminal are you referring tool?

 

Best regards,

Felipe

0 件の賞賛
返信

1,815件の閲覧回数
takeuchi_kazuhi
Contributor II

Hello Felipe
Thank you for answering my question.
I am trying to control a motor using FLEX WMA of MKV46F256VLL16.
At the same time, i am trying to communicate data using SPI and I2C.
However, looking at "KV4x Signal Multiplexing and Pin Assignments" in the KV4x Reference Manual,

I feel that FLEX WMA, SPI, and I2C cannot be used at the same time.
Is this understanding correct?
If it is not correct, how settings can be used to use FLEX WMA, SPI, and I2C at the same time?

Best regards,

Takeuchi

0 件の賞賛
返信

1,815件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Takeuchi,

 

You can use the 3 peripherals at the same time, you shouldn’t have any issue with it. Just make sure that you select different pins for each purpose. As you can see different pins are mapped with the same functionality for example PTE16 and PTA4 with SPI0_PCS0 so you can have more options.

 

I hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,815件の閲覧回数
takeuchi_kazuhi
Contributor II

Hello Felipe.

Thank you for answering my question.
I was able to understand.

Best regards,

Takeuchi