About K64F SDIO example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About K64F SDIO example

1,229 Views
wangshuhai
Contributor I

Hi~,I have some question about K64F SDK V2.2.0 _MK64F512XXX12 .I try to use K64F SDK about SDIO, then i open the "SDCARD_FAFTS" rebuild it and Connected the SD card module , but it can't worked . It really can use? I check the conncect , then use other project about SDIO,then it work,But use SDK of K64F it not work. Could you tell me how i can use the K64F SDK work, please! 

Labels (1)
0 Kudos
Reply
1 Reply

1,153 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi wang shuhai

I have tested "frdmk64f_driver_examples_sdcard_fatfs" in the SDK 2.2 and this code worked without problems in a microsd of 4GB. I cannot see the problem that you mentioned, could you confirm that the microSD taht you are using is supported by the K64F MCU.


Best Regards,
Jorge Alcala

0 Kudos
Reply