AN2295 Serial Bootloader "SlaveFrequencyCalibration()"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN2295 Serial Bootloader "SlaveFrequencyCalibration()"

1,396 Views
rabbit
Contributor III

In AN2295_Kinetis.eww, does anyone know how this function "SlaveFrequencyCalibration()" works? It doesn't work reliable.

Labels (1)
0 Kudos
Reply
1 Reply

1,252 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Rabbit,

SlaveFrequencyCalibration() is used to measures break impulse from PC and sets correct trim value, it firstly set UART RX pin as GPIO function and wait for the falling edge on it and then start to count the systick with the help of systick timer till it observes a rising edge on that pin, then it uses the result to calculate the trim value, but as the device doesn't support float point, so the final value might have some offset in some cases.

Please kindly let me know if you have any further question.

Have a nice day!!

B.R

Kan

0 Kudos
Reply