ADS Design kit model not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADS Design kit model not working

3,071件の閲覧回数
vivekexcursion
Contributor I

I`am working on designing a wideband power amplifier for which I downlaoded ADS design kit of 

MRFE6VP5150N. But this design kit doesn`t have all the files necessary for working in ADS siulation. 

Please solve my problem as I really need to work with these model.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,729件の閲覧回数
LPP
NXP Employee
NXP Employee

Typical customer's error is to install product design kit only. You must also install "RF High Power Model Design Kits (Required)".

Please, see a list of typical troubleshoots in "Overview, FAQ and Installation Instructions for ADS RF High Power Product Design Kits"
https://www.nxp.com/docs/en/company-information/OVERVIEW_MDL_ADS_DESIGN_KIT.pdf


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,249件の閲覧回数
on7yi
Contributor I

Hello,

 

I recently upgraded to ADS 2023 (student license) and unfortunately the RF power kit available on the NXP website does not work for with the 2023 version upgrade. It used to work very well with my 2016 version of ADS but it stopped working with the new 2023 version. This is a big problem as I don t want to go back using the  the 2016 version of ADS Pathwave. None of the NXP components work. I of course tried to reinstall the RF Power kit and the RF model kit but no luck :(.

Thanks

Regards

Peter

0 件の賞賛
返信