ADC0 Configuration for k70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC0 Configuration for k70

1,632件の閲覧回数
ankurchauhan
Contributor I

Hii,

I'm using twr-k70f120m kit (without MQX) with CW 10.6.4.

I'm trying to use the differential signal : PGA0DP_ADC0DP0_ADC1DP3

                                                               PGA0DM_ADC0DM0_ADC1DM3

I want some clarification on it like which channel should i use.

what should be adc mux select. bcoz differential adc pin are dedicated so i don't have to enable any gpio ??(or needed).

if anyone have any demo code on differential signal adc please share .

Thanks and regards

Ankur

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,471件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ankur Chauhan

You can select the inputs channel for the ADC with the Status and Control Registers 1 (SC1). Over there you also have to specify the operation mode (Differential or single-ended).

a.png

In ADC0, the channel DAD0 is:

aaa.png

The inputs that you mentioned (PGA0DP_ADC0DP0_ADC1DP3 and PGA0DM_ADC0DM0_ADC1DM3) can be used for ADC0 or ADC1, so please consider it.

I made this quick code for a ADC0 initialization:

void ADC0_init(void)

{

       /* Clock ADC0 */

        SIM_SCGC6 |= SIM_SCGC6_ADC0_MASK;

   

        /* Configure for Differential mode and select DAD0 (ADC0DP0/ADC0DM0)

          * default value for ADCH is DAD0*/

        ADC0_SC1A = ADC_SC1_DIFF_MASK;

       

        /* Select 16-bit conversion and low porwer enable

         *  divider 8 from the input clock to ADC16 and long sample resolution */

        ADC0_CFG1 = ADC_CFG1_MODE(0x03) | ADC_CFG1_ADLPC_MASK | ADC_CFG1_ADIV(0x03) | ADC_CFG1_ADLSMP_MASK;

       

        /* Asynchronous clock output enable */

        ADC0_CFG1 |= ADC_CFG1_ADICLK(0x03);

        ADC0_CFG2 =  ADC_CFG2_ADACKEN_MASK;

}

       

There isn´t any sample code on differential mode adc for the twr-70f120m, but you can search for the "KINETIS_120MHZ_SC", this package sample code include different demo apps for twr-70 and twr-60.

Hope this information can help you.

best regards

Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信